User Activity

Hi, i have write a code to erase data of internal flash memory of the MCU. But when i  debug it,a page(tab) pops up with the following message: No source available for "<signal handler called>() at 0xfffffffe" . And i can't any longer debug. I use th...
Hi, i have made an custom external loader for MX25L12833F-STM32L4P5. STM32CubeProgrammer gives me the following errors: "Error:failed to erase memory". Some time it gives me the error: "Error: failed to download Segment[0]", "Error: failed to downloa...
Hi, i want to convert my generated .elf file to .stldr file. I need a stldr file for CubeMX programmer, so that i can use it to program my external flash memory(write,erase, read). I have seen in the video from ST about external loader, that the ST-e...
Hi, i have done the necessary for generating an external loader(.stldr file) with stm32Cube IDE. When i compile to generate the .stldr file, i get the error "cannot find the specified linker script". In my picture, you can see that i have done everyt...
Hi, i wanted to know the following. Must Flash.Id file be edited to write/erase an external flash memory? The following is written in Flash.ID file: " Set memory bank area and size if external memory is used". How can TouchGfx know that it must write...
Kudos from