cancel
Showing results for 
Search instead for 
Did you mean: 

Use LSI or HSI as the clock source of RF unit in STM32WB55

YYoyo.1
Associate II

To use a clock to drive the RF unit of the STM32WB55, here are 2 options in the BLE_p2pServer demo code, LSE and HSE divided by 1024,

YYoyo1_0-1692235489117.png

I want to know if it is available to use LSI or HSI as the clock source of RF unit in it, thank you.

1 REPLY 1
TDK
Guru

Only LSE and HSE/1024 are available as an RF wakeup clock source on this chip per the reference manual.

TDK_0-1692236792664.png

 

If you feel a post has answered your question, please click "Accept as Solution".