cancel
Showing results for 
Search instead for 
Did you mean: 

Changes in pin assignment through the STM32 MC Workbench does not Update

Tore Kallevik
Associate II

Project generation -> "UPDATE" does not update STM32 pin assignment.

AN5166 2.4.3: The preferred way to change pin assignment is obviously through the STM32 MC Workbench.

The only way to change pin assignment through STM32 MCSDK is to select "GENERATE"

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear  @Tore Kallevik​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, and so on)?

Best regards

Laurent Ca...

Tore Kallevik
Associate II

My project is with MCSDK 5.4.6, MCU STM32G474QE and STM32CubeMX 6.1.0