User Activity

Is there a way to backup partitions or the whole contents to a file so that  it can be restored later on ? For example:any idea ? It is only a programmer then ? :)  
 This question is a based on of a support ticket due to more knowledge persons from ST may answer this on the forum. Hope someone can help.Any specific reason to use this type of LVDS connector instead of 40pin FPC ? (less costly connector and cable,...
Found the cause and solved. what happened was:1. Plugged the host PC only into the STLINK USB-C. with SW1 set to 1, the device booted from EMMC and debug data was shown on USB UART. Assumed based on the MPU running, it would be enough power for the D...
EnvironmentSTM32MP157 board using I2C touch controller: ECO  5.0Problem descriptionTouch data  reporting:[1]  evtest with the touch driver loaded: X and Y coordinates are correct [2] w/o  touch driver but I2c enabled and read I2C data from the touch ...
These are the ECCN for these processors. The code for MP1 and MP2 are different. When purchasing parts from retailer in the USA, an export authorization check was done on their website (no idea why) and retailer said they had to wait for the US agenc...