User Activity

Hello,I'm using the Unicode::snprintfFloat function with the '#' flag, which should add a decimal point even if there are not decimals. This works fine in 4.21.3, but not anymore in 4.22.0. The decimal point (.) is not written to the buffer anymore [...
Hello,Coudn't find a Bugtracker, so I posted it here.I use a static graph in my project, but after some time (adding other stuff) the TouchGFX-Designer (4.20) creates incomplete code:This happend several times, only fix is to remove and add a new dia...
Hello,I'm developing a USB-Host application (MSC / Fullspeed) with the STM32H743 µC (using STM32H743I-EVAL2 Board)The application works fine when using PLL3Q as clocksource.But when I use PLL1Q or RC48 as clocksource the USB "Core soft reset" timed o...
Hello,I tried to port an TouchGFX-Application from ARM5-Compiler (ARMCC) to ARM6 (ARMCLANG). Both compilers are from KEIL (µVision).Well it does compile, but it doesn't link:Warning: L6869W: abstractpainter.o requested the Rogue Wave Standard C++ Lib...
Kudos from