2023-09-10 09:24 AM
Hello,
I'm using the Unicode::snprintfFloat function with the '#' flag, which should add a decimal point even if there are not decimals. This works fine in 4.21.3, but not anymore in 4.22.0. The decimal point (.) is not written to the buffer anymore [ASCII '46']).
As example here is the code from your documentation:
Unicode::UnicodeChar buffer[20];
Unicode::snprintfFloat(buffer, 20, "%#6.f", 3.14159f);
// buffer=" 3."
Results:
4.21.3: " 3." (as expected) 4.22.0: " 3" (dot is missing)
2023-09-11 07:38 AM
Hello @PBull,
Indeed, I also manage to reproduce this between 4.21.4 and 4.22.0.
I'll report it to the team.
Thanks for the input 🙂