Hello,
You must first check the FFC connector (CN1) assignment with the STM32N657X0-Q board ( UM3354Camera module bundle for STM32 boards) and example DCMIPP_SnapshotDecimationMode.
Then you can dump a frame buffer in debug and to output it has a bi...
Hello,Did you already succeed with the following example in STM32CubeMx repository ?NUCLEO-H743ZI\Examples\ADC\ADC_RegularConversion_Polling.This example is a basic one with ADC1 conversion result polling.Let me know if you further information,Regard...
Hello,I would recommend you to refer to the following example with the ADC sequencer implementation. You can find it in the STM32Cube_FW_L4_V1.18.0 repository and folder \Projects\STM32L476G-EVAL\Examples\ADC\ADC_Sequencer.Let me know if you need fur...
Hello Michal,What you are observing may be relative to the Miller effect inside the comparator circuitry.Would it be possible for you to set bit#1 (not documented) in COMP_CxCSR, it enables a compare feature which hold the comparator output during th...