cancel
Showing results for 
Search instead for 
Did you mean: 

[BLUENRG-LP] Scan devices when using CODED_PHY

LTrin.1
Associate II

Hello everyone. 

I'm facing a issue when I try to use CODED_PHY instead 1M_PHY. When I start a GAP_GENERAL_DISCOVERY_PROC, the stack returns: 0xD1 (BLE_STATUS_INVALID_SCAN_CONFIGURATION).

Could anyone help me? The scan configuration is (return 0x00 - OK):

 

 

 

  ret = aci_gap_set_scan_configuration(DUPLICATE_FILTER_ENABLED, SCAN_ACCEPT_ALL, LE_CODED_PHY_BIT, PASSIVE_SCAN, SCAN_INTERVAL, SCAN_WINDOW);
  PRINTF("Scan configuration for LE_CODED_PHY: 0x%02X\n", ret);

 

 

 

and the start procedure function returns 0xD1 (NOK). variable phy = LE_CODED_PHY.

 

 

 

	ret = aci_gap_start_procedure(GAP_GENERAL_DISCOVERY_PROC, phy, SCAN_DURATION/10, 0);

	if(ret){
	  PRINTF("start general discovery failed; err: %02X", ret);
	}

 

 

 

When using 1M_PHY it works well. 

I can't see more details about the functions and error troubleshooting in the documentation, so I'm looking help here.

Best Regards,

Leonardo

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0