2022-12-08 9:38 AM
Hello everyone
I'm trying to use aci_gatt_clt_read_multiple_char_value() function but it are returning error 0x82 (BLE_STATUS_INVALID_PARAMS).
aci_gatt_clt_read() function works as expected but I want to read multiple values for optimization purposes.
Code:
void refreshDeviceParameters()
{
PRINTF("%s\r\n",__func__);
Handle_Entry_t handle_entry[DEVICE_MAX_PARAMS];
PRINTF("Handle entry: ");
for(int i = 0; i < DEVICE_MAX_PARAMS; i++)
{
handle_entry[i].Handle = i;
PRINTF("[0x%02X] = 0x%02X ", i, handle_entry[i].Handle);
}
PRINTF("\r\n");
tBleStatus ret = aci_gatt_clt_read_multiple_char_value(connection_handle, (uint8_t) DEVICE_MAX_PARAMS, handle_entry);
if (ret != BLE_STATUS_SUCCESS)
{
PRINTF("Error reading multiple char values 0x%02X\r\n", ret);
}
}Output:
refreshDeviceParameters
Handle entry: [0x00] = 0x00 [0x01] = 0x01 [0x02] = 0x02 [0x03] = 0x03 [0x04] = 0x04 [0x05] = 0x05 [0x06] = 0x06 [0x07] = 0x07 [0x08] = 0x08 [0x09] = 0x09 [0x0A] = 0x0A [0x0B] = 0x0B [0x0C] = 0x0C [0x0D] = 0x0D [0x0E] = 0x0E
Error reading multiple char values 0x82Can anyone help me please?
Regards,
Leonardo