2022-08-09 08:04 AM
Hello there
I have a custom board based on STEVAL-IDB011V2 EVM. Is the same schematic but I have a problem with this. Apparently it boots but not run...
When I flash "Hello World" example I have some issue that I can't check why.... The expected message does not is sent complete. So I have this output:
In this test, I reset the board sometimes. Some times it shows "Applicat", "Applicati", (Probably bootloader output?) Some times it shows truncated "Hello World".
I checked voltage levels by https://www.st.com/resource/en/application_note/an5503-bringing-up-the-bluenrglp-bluenrglps-devices-stmicroelectronics.pdf application note (bringing up the bluenrglp devices).
I tried the Power Supply test (flashing DTM Firmware - UART without update) and VDDA thats we expect 1.2V, I measured 0V. The Core voltage (VCAP) I measured 1.2V as expected.
I also tried flash other firmware examples without success.
Can someone help me?
Solved! Go to Solution.
2022-08-18 12:53 AM
Hi,
I just replied to your message.
I guess the problem was related to 22nH used for SMPS instead of 10uH (22nH is optional and can helps in sensitivity performances - "killing" the SMPS spurious).
Please confirm.
Regards
Laurent
2022-08-17 12:31 AM
Hello,
Could you share your schematics and associated Bill of material?
Regards
Laurent
2022-08-17 01:51 PM
Hello there
Please see you message inbox. I sent to you.
Regards,
Leonardo Trinta
2022-08-18 12:53 AM
Hi,
I just replied to your message.
I guess the problem was related to 22nH used for SMPS instead of 10uH (22nH is optional and can helps in sensitivity performances - "killing" the SMPS spurious).
Please confirm.
Regards
Laurent
2022-08-18 06:29 AM
Hello there
Yes, was it that's what caused the issue. Sorry for inconvenience.
As suggestion, clarify it in EVM schematic.
Thank you
Regards,
Leonardo
2024-01-09 11:36 AM
Hi Laurent,
I just saw this post and I'm wondering if I have an issue with my schematic as well.
Based on schematic for STEVAL-IDB011V2, there is a 22nH inductor for L4 (attached to VLXSD) and based on the datasheet DS13282-rev-6, page 11, I have a similar thing, VLXSD->22nH->(VFBSD and (4.7uF || 0.1uF) caps to ground.)
I do not have a 10nH inductor in series with the 22nH inductor as shown in the V1 schematic of UM2735 page 99). Will this cause issues with SMPS ON operation?
Thank you