Skip to main content
ABouk.1
Associate III
February 18, 2025
Solved

TESEO LIV3F no signal

  • February 18, 2025
  • 2 replies
  • 1962 views

Hello,

I have assembled a PCB that contains a TESEO LIV3F + LNA + SAW, this part of the schematics is shown below.

Using the teseo suite pro, the GPS receives no signal so I used a -9dB 1575MHz RF source on the input and measured the RF power at the output (GPS_RF_IN), the signal is well amplified and filtered but the LIV3F module cannot see a single satellite.

Any ideas pls ?

Capture d’écran 2025-02-18 082352.pngCapture d’écran 2025-02-18 082106.png

This topic has been closed for replies.
Best answer by ABouk.1

Hello,

After some days of hardware debugging, i found out that it was due to the fact that the decoupling capacitor on the LNA supply was too far, I just had to get it closer to the IC and everything was fine :)

2 replies

ST Employee
February 26, 2025

Hello,

What type of antenna are you using for GPS reception ?

Maybe it is an active one. It could explain why you have no reception.

ABouk.1
ABouk.1AuthorBest answer
Associate III
February 26, 2025

Hello,

After some days of hardware debugging, i found out that it was due to the fact that the decoupling capacitor on the LNA supply was too far, I just had to get it closer to the IC and everything was fine :)