User Activity

Hello, I'm working on a project started from Zigbee_APS_coord and Zigbee_APS_router examples on NUCLEO-WB55.USBDongle with STM32Cube_FW_WB_V1.21.0.The project is based on data exchange between the coordinator and several devices acting as routers (fr...
Hello, I'm working on a project based on NUCLEO-WB55.USBDongle. According to Zigbee specification paragraph 3.6.1.2 referring to to the NLME-PERMIT-JOINING.request procedure:When this procedure is initiated with the PermitDuration parameter set to a ...