User Activity

Continuing saga of attempting to run a TouchGFX demo on a NUCLEO-G071RB with X-NUCLEO-GFX01M2($AZ2).I connected the NUCLEO board, selected it in TouchGFXDesigner, then selected the relevant demo.Having installed the latest TouchGFXDesigner (4.24.2), ...
1.I have TouchGFX Designer 4.24.2 and STM32CubeMX running on Windows 11.  I downloaded the demos and examples via the file menu, also the latest TouchGFX Generator via CubeMX.  I am targetting a NUCLE0 STM32G071 with GFX01M2($AZ2) display, so I selec...
I have a NUCLEO -G071RB board with an X-NUCLEO-GFX01M2 display shield, and am trying to run the X-CUBE-DISPLAY demonstration software GFX01M2_HelloWorld.  I have imported the project to CubeIDE and built it OK, but when I try to run it I get an error...
Having upgraded CubeIDE to version 1.17.0 using 'check for updates' and found it didn't work for my project, I tried to go back to version 1.15.1 using the revert button.  After running this, the IDE would not start and give an error message indicati...
I've just upgraded from Cube IDE 1.15 to 1.17.0 under Ubuntu 22.04 using the 'check for updates' feature.When I try to rebuild (right click in project explorer and click 'build project') any of my existing projects I just get a message such as below....
Kudos from