sryuj.1
Associate
since
2020-12-02
2023-06-14
User statistics
3
Posts
0
Solutions
0
Kudos given
2
Kudos received
STMicroelectronics Community
About sryuj.1
Options
Report User
User Activity
Posts
Replies
When using the STMF479, if the DHIHOST function is not used, can the corresponding pins be left unconnected?
2020-12-17
When using the STMF479, if the MIPI function is not used, can the corresponding pins be left unconnected?
2020-12-17
Terminal treatment of the STM32F479BIT6 when the MIPI circuit is not used
2020-12-02
Questions about STM32F479BIT6If the MIPI circuit is unused andThe following pins are NC,pull-up,pull-downWhich terminal treatment should I use?Target Terminals119/120/121/122/122/122/124/124/125/126/127/128/
No replies to display.
Kudos from
User
Count
Legacy member
2
View all