cancel
Showing results for 
Search instead for 
Did you mean: 

When using the STMF479, if the MIPI function is not used, can the corresponding pins be left unconnected?

sryuj.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Yes, just leave the corresponding DSIHOST pins unconnected.

However, please note the information in the data sheet (Section 2.18).:

If DSI functionality is not used at all, then:

  • VDDDSI pin must be connected to global VDD.
  • VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
  • VSSDSI pin must be grounded

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.