cancel
Showing results for 
Search instead for 
Did you mean: 

When using the STMF479, if the DHIHOST function is not used, can the corresponding pins be left unconnected?

sryuj.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @sryuj.1​ ,

I advise you to refer to the STM32F479xx Datahseet relevent for your device for more clarification on DSI Host functionality.

This document will guide you to configure the pins, and you will find this detail:

"If DSI functionality is not used at all, then:

  • VDDDSI pin must be connected to global VDD. 
  • VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
  • VSSDSI pin must be grounded.

"

You have also this helpful guide AN4860 Application note DSI Host on STM32F469/479, STM32F7x8/x9 and STM32L4R9/S9 MCUs.

Hope this helps you, and please don’t hesitate to come back for more clarification or any question.

Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen