cancel
Showing results for 
Search instead for 
Did you mean: 

Terminal treatment of the STM32F479BIT6 when the MIPI circuit is not used

sryuj.1
Associate

Questions about STM32F479BIT6

If the MIPI circuit is unused and

The following pins are NC,pull-up,pull-down

Which terminal treatment should I use?

Target Terminals

119/120/121/122/122/122/124/124/125/126/127/128/

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0