User Activity

Hi,i'm using cubemx and updated from touchgfx 4.21.2 to 4.22.1 and also installed the newest touchgfx designer.After regeneration of the project certain files like TextKeysAndLanguages.hpp are missing. So all my texts are missing.i can see it in my g...
Hi,i had a programm running on the stm32f407 and PWM output via Tim2 The timer is configured with clock 84MHz and PWM Counter Period 5040 which gives me a period time of 60us. The timer is clocked via APB1. this works finenow i use an h753 with the ...
Hi,I want to switch a project in cubemx from stm32f407 to the stm32h753. (both lqfp100in cubeMX 6.8.0 there is this pinout feature to show compatible cpus. cubeMX lists me all the variants of the stm32F4, L4 and F7 but there are no H7 listed.Is there...
Hicompiling with ArmClang 6.18 generates loads of warnings.Are there any plans to fix these. It is disturbing to get these warnings as they hide other problemsI attached a file with the warnings i get in the touchGfx codebaseRegards
I try to implement a multilevel menusystem with one scrollwheel-widget and pysical buttons.I added a scrollwheel with 10 items(even if my menu has not 10 items in every level of hierachy) and want to manage the items on my own, as i want to use this ...
Kudos from
Kudos given to