User Activity

Say, I have a STM32L431RB (128k,64k) on a board design. This is the lowest flash size on the 6 chips on the STM32L4x1Rx 64pin variety. It certainty looks like I can drop-in any of the larger flash/ram chips as the pin outs all look the same. But do I...
In AN4899 it specifies that one should add a zener diode from the 5V rail to the 3.3V rail in order to have complete safety when using FT pins with 5V pull ups. Does anyone know what the specifications of the Zener diode should be (currents, resistan...
SummaryAt the end of the day, my issue is missing something in documentation. The lesson here, is test thoroughly. Just because it works for a few minutes, doesn't mean forever. Anyway, I've been running >3mA through the pins that are limited before ...
See the image. I can't figure out how I have done this, but my source folders appear like this, rather than in a hierarchy. When I open the folders in explorer, they are all nested as you would expect, folders inside folders. They are not folders wit...
Does anyone have experience with 5V pull ups? do you have to power on the 5V source after the MCU is started?I'm running a STM32L431CBT6  with external 5 volt 10k pull-ups on the pins PB11,12,13,14,15 and PA1. (all flagged as FT pins)I've been able t...