cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN interrupt on STM32G481

Nickelgrass
Senior II

Hello,

I am using STM32G491 FDCAN modules 1 and 2 in bare metal. While everything works perfectly on CAN2 the interrupt on CAN1 is constantly disabled. And I do not mean the flags but the actual interrupt does not fire. Each time the interrupt for CAN2 fires, the interrupt from CAN1 is disabled. When I read out the register NVIC->ISER[0] after initialization then I can see bits 6 (EXTI0) and 21 (FDCAN1_IT0) are set. Once FDCAN2 interrupt fires these two bits are reset to 0. I need to enable them again in the ISR of CAN2. How can this happen? How can the interrupt simply be disabled by a different interrupt?

1 ACCEPTED SOLUTION

Accepted Solutions
Nickelgrass
Senior II

Found the problem. Was unrelated to the interrupt. Why is not possible to delete useless posts?

View solution in original post

2 REPLIES 2
Nickelgrass
Senior II

Found the problem. Was unrelated to the interrupt. Why is not possible to delete useless posts?

Perhaps, put the solution and accept it as solution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.