2020-09-25 12:20 AM
HI,
I'm trying use SDIO interface on STM32F469I-Discovery board and I'm always getting FR_DISK_ERR for the command "f_open(&myfile,myPath,FA_CREATE_ALWAYS|FA_WRITE)" Same problem is observed with 1-bit and 4-bit SDIO mode. I have enabled "Use DMA template" and using FAT32 formatted 16GB Micro SD card with a sector size of 4096 bytes. And also I have enabled SDIO Global interrupt. What is the maximum size of Micro SD card supported by the STM32F469I-Discovery board?Can anyone help me in resolving the issue?
Thanks in advance
Sunil
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.