User Activity

HiI cloned a STM32Cube project that was developed on a windows 10 machine to my 18.04 ubuntu machine and opened the project.When I click on the .ioc file (and expect to get an overview of the CPU) I get a blank sheet and the laptops fan increase it's...
HiIs there a way to make a cold start(reboot) in C language in the STM32Cube Environment using a Nuclei board?In other IDE's for other CPU's it waspossible to create a function that inserted a RESET assembler mnemonic for thetarget CPU like thisvoid ...
Dear allBecause the STCS2A have separate pins for the FB and Source it is attempting to Think by manipulating the FB pin's voltage feedback to change the actual current through the leds.I tried to connect an operational amplifier between the source p...
Dear allWe are exploring to replace our current valve driver package with some 75 pieces of the VNQ5160K-E but have have some questions around the snuffer circuite for high side drivers.The VNQ5160K-E's will not operate in an automotive envionment so...
Kudos from