2023-07-24 2:08 AM - last edited on 2024-11-23 2:00 AM by Andrew Neil
Dear CubeIDE team,
I just started using CubeIDE.
Following are my question.
1. How can I find string text in .h file?
I tried to "ADC_OVR_DATA_OVERWRITTEN" string in Drivers\..\inc using "Ctrl+H" but I failed.
This is very uncomfortable to use. Now I am using ither search software due to this symptom.
(As I remember, this was very old issue. I hope you will guide me to solve this.)
2. CubeIDE 1.13.0 memory usage is too big.
I think CubeIDE is using too much memory(more than 1.1GB) compared with IAR-IDE(about 450MB at 9.xx).
My labtop has 8GB ram. this is not that big ,but not that small. But when I opened CubeIDE, I can not open the other software due to lack of memory.
Thanks in advance for your help.
Best Regards,
Kslim
2023-07-24 2:33 AM
ad 1 . why not use "find.." from menu ?
or find in files to search on project..files ? right click -> Search text..
ad 2.
this is more a windows problem : use 1GB of 8GB shoud be nothing problematic. except for Win...
see: i run Linux (MX18 , 5y old) , on 8GB , AMD quadcore 3GHz;
the ide (java ...) use up 1,5GB here, the browser (49 windows open) about 2GB -> still > 3GB free. zero problem!
and mem use:
2024-11-23 1:31 AM
I also expierienced problem number one. The search feature is completely unusefull. For example, when I need to find all occuriences USART_CR1_RE in the HAL library I need to use grep from bash console !!!
Really ? How ST could release that crappy IDE ?
For now I am using STM32CubeIde only for quick importing some examples and debugging. The most important feature searching doesnt work.
Dear ST, please fix it ASAP. My project is at early stage so really I am considering to convince my client to change platform to some NXP product.
Regards
Paweł