MDK compiles, and the program loads the following results: IDE compiles, and the program loads the following results: The MDK program is exported from the IDE, and the two programs are the sameI want to use openamp in MDK, how can I modify it
Qt uses 'eglfs' to display. After configuring this 'hwcursor', use Qt to display the card on HDMI. The touch screen will also get stuck. When the QT_QPA_GENERIC_PLUGINS environment variable is deleted and the mouse is plugged in, the mouse cannot be ...
I compiled according to St Yocto and used version 3.1.I don't use Wayland, I use EGLFS.But Qt uses EGLFS more slowly than Wayland does, and the mouse moves slowly across the screen.Using Qt version is 5.14.1.
I am in the uboot code. Use the configuration file stm32mp15_basic_defconfig. Compile SPL and uboot. Then replace flashing to SD card to start, the following situation will appearStuck here, will not boot the kernelSTM32MP157C-DK2