cancel
Showing results for 
Search instead for 
Did you mean: 

The MDK uses OpenAMP to communicate.Loading is not initialized at /dev/ttyrpmsg0.Programs are available in the IDE.

User.44
Associate II

 MDK compiles, and the program loads the following results:

0693W00000Bd8ouQAB.png IDE compiles, and the program loads the following results:

0693W00000Bd8pxQAB.png The MDK program is exported from the IDE, and the two programs are the same

I want to use openamp in MDK, how can I modify it

1 ACCEPTED SOLUTION

Accepted Solutions
ArnaudP
Senior
1 REPLY 1
ArnaudP
Senior

Hello @文�?� �?​ 

A MDK project example integrating OpenAMP library is available here:

https://github.com/STMicroelectronics/STM32CubeMP1/tree/master/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo