Skip to main content
SSala.3
Associate III
June 10, 2022
Question

Ethernet communication not working in ST32Cube IDE 1.9.0

  • June 10, 2022
  • 1 reply
  • 835 views

Hi,

I have a custom board with STM32f427VG and KSZ8041NL PHY. My ethernet communication is working well in STMCube IDE 1.8.0. But when I try to configure ethernet in ver:1.9.0 I don't see a input box for PHY address. It says it some ethernet settings has been moved to LWIP setting page.

How do I set my PHY address which is 1 in STMCube IDE 1.9.0? Is there any more setting to be done compared to 1.8.0 for ethernet communication.

Did anyone face this issue?

Thanks.

This topic has been closed for replies.

1 reply

ykn
Associate III
June 10, 2022

ST32Cube IDE 1.9.0 has some unfamiliar bug, which I faced with ADC.

my suggestion keep working with 1.8.0.