cancel
Showing results for 
Search instead for 
Did you mean: 

There is an error in STM32CubeMX which I updated yesterday to the latest version - see details below

MLane.3
Associate II

With the latest version of CubeMX (Version: 6.0.0-RC5) there is a reported error with ADC configuration. I will attached the preferred configuration below. The problem is that the latest version will not let me select ADC2, see attached configuration, for 'DMA Circular Mode'. ADC1 is ok but for some reason CubeMX will no allow ADC2 to be selected as 'DMA Circular Mode'. I can only select DR or DFSDM Mode - not circular!

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
TDK
Super User

What chip?

If you feel a post has answered your question, please click "Accept as Solution".
Stm32h743 on the Nucleo H743Z12 Get Outlook for iOS<>

Hello @MLane.3​ 

Could you please share your .ioc file to check the issue.

Best regards,

Nesrine

Hello @MLane.3​ 

Thanks for the feedback, issue reported to the tool development team that will plan the correction.

Best regards,

Nesrine

Hello @MLane.3​ 

Sorry, It's not a bug, To activate the "DMA Circular mode" it must be configured in DMA Settings Tab.

Best regards ,

Nesrine

MLane.3
Associate II

ok that fixed the problem. Why did it change though? This was fine up until I updated CubeMx.