cancel
Showing results for 
Search instead for 
Did you mean: 

I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.

mSH.1
Associate III

hello

I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.

An operation has occurred.

  • used STM32H735G-DK ​/ CubeIDE
  08:16:59 : STM32CubeProgrammer API v2.9.0
  08:17:02 : ST-LINK SN  : 004A001D3438510734313939
  08:17:02 : ST-LINK FW  : V3J9M3
  08:17:02 : Board       : STM32H735G-DK
  08:17:02 : Voltage     : 3.28V
  08:17:02 : SWD freq    : 24000 KHz
  08:17:02 : Connect mode: Normal
  08:17:02 : Reset mode  : Software reset
  08:17:02 : Device ID   : 0x483
  08:17:02 : Revision ID : Rev Z
  08:17:02 : ST-LINK SN  : 004A001D3438510734313939
  08:17:02 : ST-LINK FW  : V3J9M3
  08:17:02 : Board       : STM32H735G-DK
  08:17:02 : Voltage     : 3.28V
  08:17:02 : SWD freq    : 24000 KHz
  08:17:02 : Connect mode: Normal
  08:17:02 : Reset mode  : Software reset
  08:17:02 : Device ID   : 0x483
  08:17:02 : Revision ID : Rev Z
  08:17:02 : Debug in Low Power mode is not supported for this device.
  08:17:02 : UPLOADING OPTION BYTES DATA ...
  08:17:02 :   Bank          : 0x00
  08:17:02 :   Address       : 0x5200201c
  08:17:02 :   Size          : 92 Bytes
  08:17:02 : UPLOADING ...
  08:17:02 :   Size          : 1024 Bytes
  08:17:02 :   Address       : 0x8000000
  08:17:02 : Read progress:
  08:17:02 : Data read successfully
  08:17:02 : Time elapsed during the read operation is: 00:00:00.002
  08:17:07 : Read File: C:\TouchGFXProjects\Noble_cooker\STM32CubeIDE\Debug\STM32H735G-DK.hex
  08:17:07 : Number of segments: 2
  08:17:07 : segment[0]: address= 0x8000000, size= 0x5DA00
  08:17:07 : segment[1]: address= 0x90000000, size= 0x86691C
  08:17:15 : Memory Programming ...
  08:17:15 : Opening and parsing file: STM32H735G-DK.hex
  08:17:15 :   File          : STM32H735G-DK.hex
  08:17:15 :   Size          : 9192220 Bytes
  08:17:15 :   Address       : 0x08000000 
  08:17:15 : Erasing memory corresponding to segment 0:
  08:17:15 : Erasing internal memory sectors [0 2]
  08:17:18 : Erasing memory corresponding to segment 1:
  08:17:18 : Download in Progress:
  08:17:21 : Error: failed to download Segment[1]
  08:17:21 : Error: failed to download the File

​thank.

2 REPLIES 2

Make sure you've selected a suitable External Loader for the board, see [EL] gear/bitcoin icon on the lower left edge of the screen.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

https://www.youtube.com/watch?v=q0vbKRoLETs

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..