2022-07-31 4:18 PM
hello
I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.
An operation has occurred.
08:16:59 : STM32CubeProgrammer API v2.9.0
08:17:02 : ST-LINK SN : 004A001D3438510734313939
08:17:02 : ST-LINK FW : V3J9M3
08:17:02 : Board : STM32H735G-DK
08:17:02 : Voltage : 3.28V
08:17:02 : SWD freq : 24000 KHz
08:17:02 : Connect mode: Normal
08:17:02 : Reset mode : Software reset
08:17:02 : Device ID : 0x483
08:17:02 : Revision ID : Rev Z
08:17:02 : ST-LINK SN : 004A001D3438510734313939
08:17:02 : ST-LINK FW : V3J9M3
08:17:02 : Board : STM32H735G-DK
08:17:02 : Voltage : 3.28V
08:17:02 : SWD freq : 24000 KHz
08:17:02 : Connect mode: Normal
08:17:02 : Reset mode : Software reset
08:17:02 : Device ID : 0x483
08:17:02 : Revision ID : Rev Z
08:17:02 : Debug in Low Power mode is not supported for this device.
08:17:02 : UPLOADING OPTION BYTES DATA ...
08:17:02 : Bank : 0x00
08:17:02 : Address : 0x5200201c
08:17:02 : Size : 92 Bytes
08:17:02 : UPLOADING ...
08:17:02 : Size : 1024 Bytes
08:17:02 : Address : 0x8000000
08:17:02 : Read progress:
08:17:02 : Data read successfully
08:17:02 : Time elapsed during the read operation is: 00:00:00.002
08:17:07 : Read File: C:\TouchGFXProjects\Noble_cooker\STM32CubeIDE\Debug\STM32H735G-DK.hex
08:17:07 : Number of segments: 2
08:17:07 : segment[0]: address= 0x8000000, size= 0x5DA00
08:17:07 : segment[1]: address= 0x90000000, size= 0x86691C
08:17:15 : Memory Programming ...
08:17:15 : Opening and parsing file: STM32H735G-DK.hex
08:17:15 : File : STM32H735G-DK.hex
08:17:15 : Size : 9192220 Bytes
08:17:15 : Address : 0x08000000
08:17:15 : Erasing memory corresponding to segment 0:
08:17:15 : Erasing internal memory sectors [0 2]
08:17:18 : Erasing memory corresponding to segment 1:
08:17:18 : Download in Progress:
08:17:21 : Error: failed to download Segment[1]
08:17:21 : Error: failed to download the Filethank.
2022-07-31 4:38 PM
Make sure you've selected a suitable External Loader for the board, see [EL] gear/bitcoin icon on the lower left edge of the screen.
2022-07-31 4:52 PM
https://www.youtube.com/watch?v=q0vbKRoLETs