Hello @_AdamNtrx ? Could you please confirm which STM32 board you are using for your project? This will help us provide you with the accurate example of LWIP using FreeRTOS. Br
Hello @jzzunn Please download the latest package of STM32CubeU5 from the st.com or GitHub. Then, open the .project under Projects/B-U585I-IOT02A/Examples/MDF/ADF_AudioSoundDetector/STM32CubeIDE with your STM32CubeIDE. We recommend installing the late...
Hello @Shubha_99 , Could you please let us know which version of STM32CubeIDE you are using? I recommend updating to the latest version, v1.18.0, and using it with latest version of X-CUBE-CRYPTOLIB, which is 4.4.0 .Regards,
Hello @SONGTAOSI Since you are operating in command mode, you can indeed run the same example (CD_DSI_CmdMode_SingleBuffer) from the STM32H747I-DISCO using 1 data lane. To achieve this, you need to disable the High-Speed mode and ensure that the dis...
Hello @ALiu.12 ,
A request to add the binary demo file to st.com has been reported internally.
Internal ticket number: 204116 (This is an internal tracking number and is not accessible or usable by customers).