cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 uClinux: using SNMP for remote management of embedded device

vlad239955
Associate II
Posted on February 02, 2012 at 12:20

Here is a sample session showing some basic uses of SNMP for remote management of an STM32-based device. This session was run under uClinux on an STM322G-EVAL board with Emraft's STM-MEM add-on. (Refer to www.emcraft.com for further information on that platform.)

After reset, U-boot comes on from embedded Flash and proceeds to boot uClinux onto the board:

U-Boot 2010.03-linux-cortexm-1.3.1 (Jan 17 2012 - 16:51:54) CPU : STM32 F2 series (Cortex-M3) Freqs: SYSCLK=120MHz,HCLK=120MHz,PCLK1=30MHz,PCLK2=60MHz Board: STM3220G-EVAL board 1 DRAM: 32 MB Flash: 8 MB ...

♯♯ Booting kernel from Legacy Image at 60020000 ... ...

Linux version 2.6.33-arm1 (

mailto:psl@ocean.emcraft.com

) (gcc version 4.4.1 (Sourcery G++ Lite 2010q1-188) ) &sharp1 Tue Jan 17 17:28:16 MSK 2012 ..

init started: BusyBox v1.17.0 (2012-01-17 17:26:56 MSK) ~ ♯ From the shell prompt, I start an SNMP agent:

~ ♯ snmpd -C -c /etc/snmpd.conf -Le -fNET-SNMP version 5.6.1

Now, I am able to query my STM32 device remotely using standard SNMP tools. For instance,  here is how this is done from a Linux PC box:

[psl@pvr ~]$ snmpget -v1 -c public 172.17.5.100 .1.3.6.1.2.1.1.1.0 SNMPv2-MIB::sysDescr.0 = STRING: Linux stm3220g-eval 2.6.33-arm1 &sharp139 Thu Feb 2 14:19:32 MSK 2012 armv7ml [psl@pvr ~]$

Back to the target, and here is how I send a trap event to remote management tools:

~ ♯ snmptrap -v 1 -c public 172.17.0.212 '1.2.3.4.5.6' '192.193.194.195' 6 99 '55' 1.11.12.13.14.15 s ''I'm here''

When I check SNMP traps at the host, the trap from STM32 is reported as appropriate:

[root@pvr ~]♯ snmptrapd -C -c /home/work/psl/SF/release/snmptrapd.conf -Le -fNET-SNMP version 5.5 2012-02-02 13:52:55 192.193.194.195(via UDP: [172.17.5.100]:53140->[172.17.0.212]) TRAP, SNMP v1, community public iso.2.3.4.5.6 Enterprise Specific Trap (99) Uptime: 0:00:00.55 iso.11.12.13.14.15 = STRING: ''I'm here''

#uclinux-stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
GHITH.Abdelhamid
Associate II
Posted on February 06, 2012 at 00:22

Hello Vladimir,

Very impressive, in how much time did it start? How much Flash, RAM is required to run this version of uClinux kernel (2.6.33-arm1)? why are you not using v2.6.36-uc0?

BR,

LN