uClinux running on STM32F437
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-05-28 1:42 PM
Posted on May 28, 2013 at 22:42
Take a look at the video below, which shows Linux, in its uClinuxform, running on the STM32F437 microcontoller:
http://www.youtube.com/watch?v=_uO8KfhfY2Y&feature=youtu.be
The novelty of this configuration is that, using the recentlyannounced STM32F437 device, the entire Linux image is able to fitinto the 2MB on-chip Flash. This has two important implications: o) Very fast boot-up times. For instance, a Linux configurationwith Ethernet and full TCP/IP stack enabled comes up in just 1second, from power-on to a point where TCP/IP is fully configuredand shell commands can run. This is pretty cool actually, by any measure. o) Entire kernel runs from the fast zero wait-state on-chip Flash,resulting in high performance of the critical system code, includingeveryhing - core kernel, TCP/IP stack, device drivers, etc. As asimple benchmark, the kernel reports ~157 BogoMIPS on a 168MHzSTM32F4:Calibrating delay loop... 87 BogoMIPS (lpj=784384)
The demo captured in the video was run on Emcraft's ''STM32F4 LinuxStarter Kit'' hardware platform:
#uclinux-stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-07-02 2:26 PM
Posted on July 02, 2013 at 23:26
Hi,
for 41$ there is also a full featured raspberry PI board or Beagleboard with 256MB/512MB Ram. I don't understand where the benefit is. Because the other Boards with Cortex-Axx are more powerful and they have full Linux ports running where adding QT4 for HMI applications is possible. Kind Regards