Posted on May 17, 2011 at 14:26 Thks for the quick reply. 1.- But how can i distinguish to this different columns that I?ve marked with red square? 2.- If i do GPIO_PinRemapConfigGPIO the pins gets multiplexed so then I can configure them?
Posted on May 17, 2011 at 14:21I know the reason. I was programming with STlink JTAG debugger and it must be done with SIMULATOR or altmost it works only in that way for me.
Posted on May 17, 2011 at 14:21 I do like you said me but that is the only i can see. I dont want this. I want code like: MOV AL, 061h and I only see the following. What am I doing wrong?? I´ve checked Project/options/C-C++Com...
Posted on May 17, 2011 at 14:16I´ve copied STM32f10xFWLIB complety. In the new examples, there is not stm32f10x_lib.h. In this file, the code includes some ST libraries header files, if they are been used, with stm32f10_conf.h. In the new one the ow...