2011-01-10 9:07 AM
IAR about question
2011-05-17 5:21 AM
As far as IAR goes,
I have used it for AVR and this is how i saw the assembly file: DEBUG or SIMULATE under PORJECT->OPTION->DEBUGGER under SETUP tab, Select Driver to be SIMULATOR or your debugging tools. Once simulation is in process, go VIEW-> DISASSEMBLY Hope this helps.2011-05-17 5:21 AM
It isn´t right and i want to see the ASM code. How can i see that on IAR
Wouldn't going to Project -> Options, and selecting ''C/C++ Compiler'' and the ''List'' tab, and then checking the ''Output list file'' or ''Output assembler file'' options and sub options, do the job?2011-05-17 5:21 AM
yes it does :).
I just do it the other way because it becomeseasier for me
to know exactly what line of code equates to the assembly when I right click on the C code -> Set Next Statement. Both works .2011-05-17 5:21 AM
I do like you said me but that is the only i can see. I dont want this. I want code like:
MOV AL, 061h and I only see the following.
2011-05-17 5:21 AM
I know the reason. I was programming with STlink JTAG debugger and it must be done with SIMULATOR or altmost it works only in that way for me.