Skip to main content
loeffel2
Associate III
March 11, 2013
Question

ADC channel match

  • March 11, 2013
  • 1 reply
  • 678 views
Posted on March 11, 2013 at 14:13

Hi

We figured out some ADC channel miss match on STM32F100C8 device, which we couldn't explane. We use the following test setup:

- ADC1_IN0 (PA0) to ADC1_IN3 (PA3) are used.

- Regular group scan mode with DMA is used.

- VDDA = 3.300V is used as reference. 

- All for channel are connected together to a OP buffer as common source.

- ADC cloch 12MHz with 55.5cycle sample time.

We got the following test results:

- ADC channel nois is fine +/- 1LSB.

- ADC1_IN1 is fine +/- 1 LSB compared to measured input voltage.

- All other channels are void -10LSB compared to measured input voltage.

- Changing the order within the regular group sequence had no influence.

- Incresing the sample time to 239.5cycle had no influence.

- Disconnecting ADC1_IN0 had no influence (To avoid voltage glitch related to the errate sheet)

- Reducing the ADC clock to 1.5MHz had no influence.

Thasnk for any help in advance.

Raphael

#adc
This topic has been closed for replies.

1 reply

loeffel2
loeffel2Author
Associate III
March 11, 2013
Posted on March 11, 2013 at 17:47

Hi

Only channel ADC1_IN1 was initialized proper. All other channels were still initialized as digitial input with pull down enabled.

Best regards

Raphael