2017-11-20 4:56 AM
Hi
I'am trying to migrate existing SPL based flash erase and program code to LL. Some flash routine are part of the xxx_ll_system driver but I am missing the erase and program routines such as the FLASH_ProgramWord routine of the SPL. Has anybody an Idea if this routine still exist in the LL or where I can find them?
At the moment I am working with STM32F100 and STM32F301 devices.
Thanks in advance. Raphael
2017-11-20 8:07 AM
Hi
Loeffel.Raphael
,Unfortunately, in the current cube packages there is no support for flash LL.
I will ask our team if there is a plan to add this, and come back to you when I have further details.
-Nesrine-
2017-11-20 11:18 PM
Hi Nesrine
Getting a timeline would be nice to plan our activities.
Thanks Raphael