Posted on May 17, 2011 at 12:24I hope, this module interest You: MMstm32F103VB minimodule * Complete, ready to use microprocessor system * Fast ARM microcontroller STM32F103Vx with up to 90 DMIPS throughput * SerialFlash memory M25P64 64Mb (8MB) ...
Posted on May 17, 2011 at 12:24Minimodule with ARM Cortex-3 32-bit microcontroller STMicroelectronics STM32F103RB (128 kB Flash, 20 kB SRAM). Include USB, CAN interface and 8MB SerialFlash. - Complete, ready to use microprocessor system - Fast ARM m...
Posted on May 17, 2011 at 11:52F-LINKcable is a cheap programmer/debugger for ARM microcontrollers STMicroelectronics family. It is compatible with FlashLink JTAG. Programmer is connected to PC through parallel port, connection with target circuit i...
Posted on May 17, 2011 at 09:52F-LINKcable is a cheap programmer/debugger for ARM microcontrollers STMicroelectronics family. It is compatible with FlashLink JTAG. Programmer is connected to PC through parallel port, connection with target circuit i...
Posted on May 17, 2011 at 09:50MMstr912 minimodule * Complete, ready to use system based on ARM9 STR912 microcontroller * STR912 - ARM966E RISC core, up to 96MHz with Ethernet controller * Ethernet PHY STE100P * Onboard 8MB serial Flash memory *...