cancel
Showing results for 
Search instead for 
Did you mean: 

New STM32F103RB module to BUY

okulicz
Associate II
Posted on June 02, 2008 at 08:03

New STM32F103RB module to BUY

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
okulicz
Associate II
Posted on May 17, 2011 at 12:24

Minimodule with ARM Cortex-3 32-bit microcontroller STMicroelectronics STM32F103RB (128 kB Flash, 20 kB SRAM). Include USB, CAN interface and 8MB SerialFlash.

0690X00000602gcQAA.jpg

- Complete, ready to use microprocessor system

- Fast ARM microcontroller STM32F103Rx with up to 90 DMIPS throughput

- SerialFlash memory 64Mb (8MB)

- Reliable reset circuit

- Built-in system generator 8MHz

- Built-in 32.768kHz crystal resonator for RTC

- Built-in voltage regulator 3.3V 400mA

- Module supply voltage: 3.3V or 3.8 - 16V

- 2 x 32 terminals with 0.1'' (2.54mm) pitch fitting every prototype board

- Small dimensions: 40.5mm x 35.5mm

- Available evaluation board and sample applications

http://www.propox.com

[ This message was edited by: okulicz.andrzej on 22-02-2008 09:50 ]

tta
Associate II
Posted on May 17, 2011 at 12:24

looks really cool :

http://www.propox.com/products/t_174.html

only (tiny) issue is we need to make an adapter so our JTAG debuggers can snap in, no direct fit :)

I also suggest you make a 48 and 100 pin board like this ??

[ This message was edited by: tta on 25-02-2008 09:52 ]

okulicz
Associate II
Posted on May 17, 2011 at 12:24

I hope, this module interest You:

0690X00000602ghQAA.jpg

MMstm32F103VB minimodule

* Complete, ready to use microprocessor system

* Fast ARM microcontroller STM32F103Vx with up to 90 DMIPS throughput

* SerialFlash memory M25P64 64Mb (8MB)

* Built-In JTAG 20-pin connector (Wiggler compatybile)

* Reliable reset circuit

* Built-in system generator 8MHz

* Built-in 32.768kHz crystal resonator for RTC

* Built-in voltage regulator 3.3V 400mA

* Module supply voltage: 3.3V or 3.8 - 16V

* 2 x 40 terminals with 0.1'' (2.54mm) pitch fitting every prototype board

* Small dimensions: 61mm x 37.5mm

* Available evaluation board and sample applications

http://www.propox.com/products/t_186.html?lang=en

:o :o :o :o :o :o :o :o