cancel
Showing results for 
Search instead for 
Did you mean: 

Programer for ARM STR9, Flash PSD, uPSD and DSM. Compatible with FlashLink

okulicz
Associate II
Posted on May 03, 2008 at 08:37

Programer for ARM STR9, Flash PSD, uPSD and DSM. Compatible with FlashLink

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
okulicz
Associate II
Posted on May 17, 2011 at 09:52

F-LINKcable is a cheap programmer/debugger for ARM microcontrollers STMicroelectronics family. It is compatible with FlashLink JTAG. Programmer is connected to PC through parallel port, connection with target circuit is done through 14-pin FlashLink standard or standard 20-pin JTAG connector by adapter added to programmer.

Features

- Supports STR91x, Flash PSD, uPSD and DSM ARM microcontrollers family from STMicroelectronics.

- Compatible with FlashLink JTAG

- Available free software: CAPS and PSDsoft express

- 14-pin connector for target circuit and standard 20-pin connector by Adapter

- Operates with target voltages in the range of 3 - 5.5 V

- Supplied from the target circuit, no need for external power supply

- Connection with PC through parallel port

Supported devices

- STR9 Family

- Flash PSD Family

- uPSD Family

- DSM Family

0690X00000603HTQAY.jpg

http://www.propox.com/products/t_181.html?lang=en

:o :o :o :o :o :o :o :o :o

[ This message was edited by: okulicz.andrzej on 03-05-2008 12:08 ]