User Activity

Dear all, I am developing motor control system, and would like to observer the (motor) current response.  In the past, the method I often used was DAC, where the current command and actual value were output separately through the DAC to an oscillosco...
Dear All, I want to use STM32CubeMonitor to monitor 64-bit variables, such as int64_t or uint64_t. However, it seems that 64-bit variables cannot be selected from the variable list (they are not displayed).Is there any way to achieve this?Best Regard...
Dear All,I've been using MCU/DSP-related products for over 10+ years, but I've always had some confusion about clock multipliers and dividers. I'd like to ask for everyone's opinion on this topic.As shown as below figure (it's the clock configuration...
Dear All,I am developing a motor control system(FOC) with STM32H5.In the FOC process, while completing the ADC conversion for current measurement, it enters the ADC interrupt, where I read the TIM2 counter(for Encoder interface) to obtain rotor angle...
Dear Sir,When I monitor the data, sometimes the value often accompanied by spikes, such as followed figure. In my case, I monitor 3 variables that update from ADC registers.Normally, their values would be around 0.The signals of ADCvalue[0] and ADC V...
Kudos from