2009-12-10 3:59 AM
STM8S105 Flash Read/Write Access Speed (sanity check for slow access)
2011-05-17 6:06 AM
Operation: 1 byte write takes 3.6ms - see code sequence below
FLASH_Unlock(FLASH_MEMTYPE_DATA); FLASH_EraseByte(flash_address); FLASH_ProgramByte(flash_address, value); FLASH_Lock(FLASH_MEMTYPE_DATA); return(value); Operation: 1 byte read takes 3 ms - see code sequence below FLASH_Unlock(FLASH_MEMTYPE_DATA); value = FLASH_ReadByte(flash_address); FLASH_Lock(FLASH_MEMTYPE_DATA); return(value); Setup of clk HSI is 16Mhz Fcpu is 4Mhz Question 1) Should the unlock/erase/write/lock cycle take approximately 3.6ms 2) Should the unlock/read/lock cycle take approximately 3.0ms - seems very long 3) To read the data memory flash do I need to unlock the flash2011-05-17 6:06 AM
All,
Re: Answer to my question 1) Reading flash does not require the unlock 2) Reading flash is fast -0 microseconds as expected 3) The STM8S has the RWW ability so to write one byte is very fast if you only write one byte and move to other code functions 4) In the STM8S to write two bytes you move from micro seconds to milliseconds2011-05-17 6:06 AM
Hi
tprog: Standard programming time(including erase) for byte/word/block (1 byte/4 bytes/128 bytes) = 6.6 ms Regards mozra