Posted on May 17, 2011 at 15:06All, Re: Answer to my question 1) Reading flash does not require the unlock 2) Reading flash is fast -0 microseconds as expected 3) The STM8S has the RWW ability so to write one byte is very fast if you only write one ...
Posted on May 17, 2011 at 15:06Simulation of timers is not supported - to the best of my knowledge. I just use a dummy PCB running and powered by my USB pod - you can develop and test but no simulation.
Posted on May 17, 2011 at 15:06I love it when windows crashes. I am running parallels under MAC os with WIndows XP - SP3 and have the same blue screen driver fault you are describing. It is a hard kill to my system. I thought this may be a Mac/Paral...