Posted on May 17, 2011 at 15:07Hi, The printf() function as it defined in the library stdio call the putchar() function to send data on the console, In your case you have personalized the putchar() function to send characters to the COM (HyperTermin...
Posted on May 17, 2011 at 15:07Hi, refer to Table 34. HSI oscillator characteristics in the last datasheet(rev4) page 62 Accuracy of HSI oscillator = 16MHz +1% this value is guaranteed by design, not tested in production. Regards mozra
Posted on May 17, 2011 at 15:07Hi, I think that is a security mechanism that is consist to write first the CCR2H register before the CCR1H. Regards Anis
Posted on May 17, 2011 at 15:07 you can do it, but you can specify your network path run the command regedit and in the HKEY_LOCAL_MACHINE>Software>FLEXlm License Manager folder create new file: - Value name: COSMIC_LICENSE_FILE - Value data: your ...
Posted on May 17, 2011 at 15:06Hi, you can update your cosmic path(Tools>Options>Toolset>Root path) as following C:\Program Files\COSMIC\CXSTM8_16K (remove Lib directory from the path) Regards mozra