2018-03-15 11:23 PM
I have been using ST Visual Develop with the STM8 Cosmic Compiler on a Virtual PC with Win10 for months.
Now I want to use it on my normal PC (also Win 10 64 bit Version 1709), CosmicCompiler is working but I cannot program the code on the target (see picture), this happens a soon as I open in the menu Tools->Programmer.
I installed the ST-Link utility and the ST Visual PÃœrogrammer, both can be started. The ST-Link V2 is correctly shown in the Device Manager of Windows.
I re-installed ST Visual Develop but this doesn't help.
Any ideas what is going wrong?Solved! Go to Solution.
2018-04-03 7:05 AM
Hello,
Yes, issue already known.
See this post for a workaround :
2018-03-30 11:14 AM
Same here...
After selecting Tools->Programmer, I get:
2018-04-03 7:05 AM
Hello,
Yes, issue already known.
See this post for a workaround :
2018-04-04 1:54 AM
Thank you!
Issue sovled!
Raivo
2018-04-04 2:30 AM
Thank you, this was the right workaround.
2023-09-19 11:09 AM
This link doesn't work
2023-09-19 11:38 AM
See this post: Any tips to solve this APPCRASH ntdll.dll error?