2021-05-09 5:51 PM
As soon as I add USART initialization, SPI starts sending data using LSB and receiving with MSB(as it was intended) bit order.
SPI init code:
/* SPI configuration */
SPI_DeInit();
/* Initialize SPI in Slave mode */
// SPI_Init(SPI_FIRSTBIT_LSB, SPI_BAUDRATEPRESCALER_2, SPI_MODE_SLAVE, SPI_CLOCKPOLARITY_LOW,
SPI_Init(SPI_FIRSTBIT_MSB, SPI_BAUDRATEPRESCALER_2, SPI_MODE_SLAVE, SPI_CLOCKPOLARITY_LOW,
SPI_CLOCKPHASE_1EDGE, SPI_DATADIRECTION_2LINES_FULLDUPLEX, SPI_NSS_HARD,(uint8_t)0x07);
SPI_ITConfig(SPI_IT_RXNE,ENABLE);
SPI_ITConfig(SPI_IT_TXE,ENABLE);
SPI_Cmd(ENABLE);
UART init code:
UART1_DeInit();
UART1_Init((uint32_t)1000000, UART1_WORDLENGTH_8D, UART1_STOPBITS_1, UART1_PARITY_NO,
(UART1_SyncMode_TypeDef)(UART1_SYNCMODE_CLOCK_ENABLE | UART1_SYNCMODE_CPOL_LOW |UART1_SYNCMODE_CPHA_MIDDLE |UART1_SYNCMODE_LASTBIT_ENABLE),
UART1_MODE_TXRX_ENABLE);
UART1->BRR2 &= (uint8_t)(~UART1_BRR2_DIVF);
UART1_Cmd(ENABLE);
2021-05-12 4:32 AM
What does the rest of the code look like? Initialization only doesn't seem to do anything, although I have never seen anyone using the USART as a SPI peripheral. And how are the USART and the SPI connected? To what?
2021-05-13 10:44 AM
The rest of the code is, in theory, not so important, as it works correctly until the UART is initialized.
In the end, I replaced UART as SPI with software SPI. However, I found a bug that led to this strange behavior. CS was not connected and, as a result, was constantly active(although this is not prohibited).
As for the task description, I make a "layer" between the sensor and another MCU. So I need to communicate with the sensor as the master and process requests from another microcontroller over the same protocol as the slave... Strange, but that's the task. =)
2023-01-10 8:08 AM
"I am facing the similar issue too but i can monitorize data i send to motor driver."
I am using g431rb and sabertooth 2x32 to drive motors. UART handles communication between these two devicesbut i need to control LED Strip also and i am using SPI for that. I can control them seperately it is really easy but when i want to run motors and turn on the led strip in the same time, i cant drive the motors. They never move but i am monitoring data (which i sent to ride to motors) with arduino serialthrough application. i have to make them work together, I am also looking for solution for this problem.
Let me know if you have any question about my issue.