STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am getting my MV values in ADC as 268 but for my requirements it should read vge equivalent to 1.31 but I am getting only 0.8 with Vref 3.3v.Can any help me with my configuration is correct .What is my mistake here please

/* MAIN.C file *  * Copyright (c) 2002-2005 STMicroelectronics */#include "stm8s.h"#include "stm8s_clk.h"#include "stm8s_adc1.h"void Clk_Config(void);void ADC_Config(void);void ADC_Read(uint16_t *MV);main(){ unsigned short MV; Clk_Config(); ADC_Confi...

SRAM.11 by Associate III
  • 970 Views
  • 0 replies
  • 0 kudos

While creating a project and adding necessary libraries with STM8s003f I am getting error in library.c files #error cpstm8 libraries\src\stm8s_adc1.c:91(14) missing prototype #error cpstm8 libraries\src\stm8s_adc1.c:92(14) missing prototype

If I commented these lines again error is notified in Clk.c file and repeated for other.My question is, if commenting all those lines will reflect any issues in building the code

SRAM.11 by Associate III
  • 979 Views
  • 2 replies
  • 0 kudos

Resolved! STM8S003F3P6's PB4 and PB5 don't go high on custom board

Hi everybody,I'm using an STM8S003F3P6 on a custom board and a not original ST-Link V2 (which works fine), and I'm trying to set high the PB4 and PB5 pins. I don't know why, but it doesn't work as it should. I put my code down below.I also wrote anot...

Some questions about ADC in SMT8S.

Hi, everyone. I have been working with STM8S, i am did not work with this microcontroller before, i have some questions about ADC (i am using STM8S103F3). 1) The first problem that i had was about the values read, i am initialize the peripheral for w...

VPatr.2 by Associate II
  • 1079 Views
  • 0 replies
  • 0 kudos

Integrated development environments for STM8 mcu on linux?

Hello everyone,I'm new on STM and I find myself having to use the STM8 in a linux environment and I saw that ST provides its IDE only for Windows.I would like to know where to find an IDE + software programmer (using ST-LINK V2) where to develop soft...

Diego1 by Associate II
  • 2867 Views
  • 3 replies
  • 0 kudos

Where do I get "STM8S standard firmware library"?

The "STM8S standard firmware library" is referenced in UM0834 for STM8S-Discovery. The library examples were well organized according to the descrription and included everything for the quick start. There were timers examples, ADC, SPI, I2C, UART exa...

SVino.4 by Associate II
  • 2055 Views
  • 3 replies
  • 0 kudos

In stm8s0003f3 ,I am reading analog voltage.I am getting the value in watch as 1544,which is not expected .Can some one help what may be the fault in the code. supply vge is 1.8v

void Init_ADC(void) {    ADC1_DeInit(); ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D2,         ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,DISABLE);  }void ADC_Read(unsigned int MV) { ADC1_...

SRAM.11 by Associate III
  • 826 Views
  • 2 replies
  • 0 kudos