STM8S001j3 programming using Arduino
Hi Iam student and I now only about Arduino but now I have a project to be creat by using stm8s001j3 so please help me how to connect my STM to Arduino IDE specifically stm8s001j3 and how to use its I2C
Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
Hi Iam student and I now only about Arduino but now I have a project to be creat by using stm8s001j3 so please help me how to connect my STM to Arduino IDE specifically stm8s001j3 and how to use its I2C
I'm finding a window between 1.47V and 1.5V where the device is consuming 1mA (as opposed to <50uA) this is only apparent when the voltage is rising and I assume the device trying to power on. The documentation states it has zero power on reset but t...
I am using a NUCLEO-S8208RB to develop UART1 communication in half-duplex, single-wire mode. The device receives messages (packets of bytes) using the UART1_IT_RXNE_OR interrupt. The next step would be to transmit a byte packet in response, without a...
When in unidirectional Transmit-only mode, how can I use MISO pin as generalpurpose I/O whithout disturb the SPI?Thanks for any help
I have used IdeaSTM8 for 3+ years with great success ... but this morning my project wouldn't compile, appearing to indicate that all functions were undefined. The only anomaly I see is that the Fileview / Source Files list has turned all my .c files...
Good morning, everyone,given the dramatic situation on semiconductor availability and sourcing, I would like to know what the future holds for the STM8 family.Supply times at distributors are discouraging, to say the least, and the official ST websit...
I'm using IAR 1.42.3 And I'm using Discovery kit with STM8S003K3 MCU.I try to use the debug of Discovery kit in IAR but don't work.When i use the ST Visual Develop using cosmic the debug works so good.
I can't seem to figure out what I've done wrong. Trying to do a single ADC conversion on the STM8L051F3 using pin PC4 but I'm just getting 0xFFFFD. Here's my ADC related code can anyone spot where I've gone wrong?void ADC_Init() { CLK_PCKENR2 |= ...
STM8L001J3. I am trying to use stvd. Downloaded the archive "STM8L15x/16x/05x/AL3Lx/AL31x standard peripheral library" . But it doesn't have my microcontroller. In which archive can I find a project for it? Tell me where can I download it?