2020-06-02 10:16 PM
When i choose the option of "ST Assembler linker" in C Compiler it compiles the code but the code is not burn in MCU successfully. And when STM8 cosmic is selected there is an error while compiling
" The command: "cxstm8 +mods0 +debug -pxp -no -pp -l -iinc -i"C:\Program Files\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c" has failed, the returned value is: 1
exit code=1.
".
License problem is "flexnet license finder" which asks for the license. Which i do not have?
Kindly, revert back