2021-03-09 2:16 AM
Hi Guys, i am using STM8S003F3 controller and i want to that how can i achive 0.1v accuracy when my ADC resolution is 1023 and my total count is 2000.
2021-03-09 5:13 AM
Read the datasheet / reference manual of the STM8.
Absolute resolution is reference voltage divided by number of steps.
2021-03-09 8:52 PM
yes you are right 5/1023=4.9mV and step size is total count/2^n-1=2000/1023=1.955.so i can get this accuracy but i want to know is there anyway to get 0.1v accuracy ??
2021-03-10 2:03 AM
> ... and my total count is 2000.
I don't know what you mean with that.
Check the datasheet for Vref options. Vref is not necessarily Vdd or Vdda.
Otherwise, you can only get Vref/2^n, i.e. Vref/1024 for the 10-bit ADC your controller has.
> ... but i want to know is there anyway to get 0.1v accuracy ??
Do you really mean 0.1V meaning 100mV ?
Then just scale down the result.
2021-03-10 2:12 AM
Also confused here, how can a 10-bit value be 2000?
Or are you averaging 2000 samples? In which case I don't understand your computation.
2021-03-10 4:19 AM
2000 count is not an ADC value it is my total input count that is +1000 and -1000 input volt mean total 2000count.
2021-03-10 4:20 AM
how do i scale it? any sample do u have??
2021-03-10 4:22 AM
It is still not clear where you pull that number from.
In relation the 10-bit ADC, this is nonsensical.
2021-03-10 4:28 AM
You have a 2KV swing on the input!! I don't expect you're going to be able to do that directly, or get the accuracy/precision with that few bits on your ADC
2021-03-10 4:40 AM
that +1000 and -1000 is my input range that i will apply to the ckt.i t will come from by user end.