cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Post-Training Quantization: 'Axis 2 is out of bounds for array of dimension 2' and Initializer Warnings with ONNX Model

Marianna
Associate

Hello! I trained a neural network in MATLAB that requires an input instance of 30 features and exported it in ONNX v7 format. I am performing post-training quantization on the ST Edge AI Developer Cloud, but I am encountering issues when trying to load the dataset to check the accuracy obtained after quantization. To save this dataset in .npz format, I am using this Python script:

_____________________________________________________________

import numpy as np
import scipy.io

x_test = scipy.io.loadmat(r'C:\Users\maria\Desktop\x_test.mat')
y_test = scipy.io.loadmat(r'C:\Users\maria\Desktop\y_test.mat')
x_test = x_test['x_test']
y_test = y_test['y_test']
x_test = x_test.astype(np.float32)

np.savez("mydata.npz", x_test=x_test, y_test=y_test)

_________________________________________________________________

x_test is a matrix that contains 102 rows (number of instances) and 30 columns, while y_test is an array of 102 rows that contains the labels of the instances.
When I try to launch the quantization in the terminal, I get this error:

 

Executing with:  {'model': '/tmp/quantization-service/3856047a-9e80-44aa-a904-d4a5d551aab9/NeuralNetwork_TreIMU_Provaaa.onnx', 'data': '/tmp/quantization-service/3856047a-9e80-44aa-a904-d4a5d551aab9/mydata.npz', 'disable_per_channel': False}

Preprocess the model to infer shapes of each tensor

axis 2 is out of bounds for array of dimension 2

 

2025-02-20 12:15:23.551235: I tensorflow/core/util/port.cc:113] oneDNN custom operations are on. You may see slightly different numerical results due to floating-point round-off errors from different computation orders. To turn them off, set the environment variable `TF_ENABLE_ONEDNN_OPTS=0`.

2025-02-20 12:15:23.579012: I tensorflow/core/platform/cpu_feature_guard.cc:182] This TensorFlow binary is optimized to use available CPU instructions in performance-critical operations.

To enable the following instructions: AVX2 AVX512F AVX512_VNNI FMA, in other operations, rebuild TensorFlow with the appropriate compiler flags.

2025-02-20 12:15:24.757973523 [W:onnxruntime:, graph.cc:1231 Graph] Initializer input_Scaling appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758000628 [W:onnxruntime:, graph.cc:1231 Graph] Initializer input_Shift appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758005838 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_1_MatMul_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758009891 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_1_Add_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758013833 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_2_MatMul_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758017604 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_2_Add_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758021321 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_3_MatMul_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

2025-02-20 12:15:24.758024952 [W:onnxruntime:, graph.cc:1231 Graph] Initializer fc_3_Add_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.

 

I don’t understand the reason for the “axis 2 is out of bounds for array of dimension 2” error because, in my network, I work with a two-dimensional matrix, and I don’t understand why it would try to access a third dimension. Additionally, I don't understand why it warns me that the initializers appear in graph inputs because I'm fairly sure they were exported as constants.

At this point, I don't know if the error is in the network or in the .npz dataset. How can I resolve this?

I am attaching the exported network.


Thank you in advance for your help!

1 ACCEPTED SOLUTION

Accepted Solutions
Julian E.
ST Employee

Hello @Marianna ,

 

it seems that you need to create a npz file with a shape of (batch_size,1,1,30) for your x_test and (batch_size,1,1,3) for your y_test.


Note that because your model is very small, the quantization makes it bigger (5.7kiB to 7.9kiB).

It adds quantize and dequantized nodes everywhere, but the benefit of quantizing your weights to int8 is smaller that the drawback of adding these nodes:

JulianE_0-1740144886132.png

I would advise you to test both your quantized and non quantized models on the benchmarking tool to see which one is better for you in terms of execution time and memory footprint.

It should be similar I think, so maybe, not quantizing is maybe better as you will not loose accuracy because of the quantization.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Julian E.
ST Employee

Hello @Marianna ,

 

it seems that you need to create a npz file with a shape of (batch_size,1,1,30) for your x_test and (batch_size,1,1,3) for your y_test.


Note that because your model is very small, the quantization makes it bigger (5.7kiB to 7.9kiB).

It adds quantize and dequantized nodes everywhere, but the benefit of quantizing your weights to int8 is smaller that the drawback of adding these nodes:

JulianE_0-1740144886132.png

I would advise you to test both your quantized and non quantized models on the benchmarking tool to see which one is better for you in terms of execution time and memory footprint.

It should be similar I think, so maybe, not quantizing is maybe better as you will not loose accuracy because of the quantization.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Marianna
Associate

Thank you so much for your help, I will follow your advice!

Now that I understand how to quantize using my dataset, I have another question. After performing quantization and optimization, I noticed an increase in memory usage and inference time. Is there a way to visualize how much the accuracy decreases, or is this something I have to calculate by observing how the network responds to the test dataset I used for the non-quantized network?